Other Parts Discussed in Thread: ADC32RF44
Hi-
We are using a ADC32RF44 EVM board on the TSW14J56 EVM host board.
We are using the supplied TI software for each board.
Are there instructions on how to set the frequency of the ADC on the ADC32RF44 board, and then have that frequency carry over to the TSW14J56? We enter a frequency into the "ADC Output Data Rate" Gui box, but believe the JESD rate is not updated as we would expect.
We have tried using internal clocking as well as external clocking.
For example, we use external clocking of 2.4GHz and set the GUI for the ADC32RF44 to be external clocked, and set the 2.4GHz value into the ADC Output Data Rate GUI on the TSW14J56. Our RF input frequency to the ADC is 300 MHz. With this set up, the detected frequency is 293.555MHz instead of 300 MHz. So something is off, likely by the same ratio as our clock shift from the 2457.6MHz (default) to the new 2.4GHz.
What is the procedure for setting a new clock frequency? Do we need to supply the JESD clock rate in the GUI? Or do we need to supply analog connection onboard somewhere?
Thanks.
Bill