Part Number: ADC10D1500RB
Hi
I have several questions to refer to you expert
1. Is the FFT computation of WAVEVISION5 implemented in my PC or on the FPGA board? If on the PC, can I program the FPGA to achieve the 8k point FFT and then transmit the spectrum data into my PC?
2. And is any firmware coding manual for the board to download, so that I can know how to deal with the acquired data in the memory, and avoid my FPGA coding overwriting the firmware already on the board?
3. If I want to call the functions in the GUI (like finding the board, trigger, sampling, etc), can I get some programming library (like C++) of TI for the board to call these functions? I don’t need the GUI. Because I want to trigger my signal source and simultaneously trigger the sampling of 8k points in a “for loop” 10k times per second, I think programming is more convenient. Moreover, the response rate of the GUI is far more slower than my application, which seems can only be solved by programming.
Thanks sincerely for your help.
Best
Jinxi