Other Parts Discussed in Thread: AFE7225
Hello,
I am currently working with the AFE7225 EVM and am trying to put the device into 'RX-TX loopback' mode so that I can inject an analog signal into the INA+ (J3) SMA Connector and look at the signal output on the 'IOUTA' (J5) SMA connector to just verify that the IC itself is working as expected. I have modified the EVM to bypass the U2 CDC IC and am feeding in two single-ended clocks into the CLKINP / CLKINN SMA connectors (J18 / J19) to try to streamline the setup. I also tried to bypass the entire TX/RX processing chain so it was as simple as possible.
The board modifications are as follows:
1) Install R112, R74 and remove R76 (per note in EVM guide, pg 13, section 6.4)
2) Install SMA connection into J19 and install R161
3) Remove T9 transformer and bridge pins 3 - 4 so that the CLKINP signal goes straight to C51
4) Remove R78 and R81
Once these mods were done, I have confirmed that I have good clocks (with the appropriate levels) at IC pins # 8 & 9 (CLKINP = ADC_CLK and CLKINN = DAC_CLK per datasheet, pg. 45)
Register Settings:
(all registers set from EVM GUI, version 1.3)
'0x20' written to address '0x20A' (Single Ended Clock mode setup)
'0x03' written to address '0x105' (RX_TX_LPBK Mode)
'0x60' written to address '0x103' (TX_Byp)
'0x60' written to address '0x167' (RX_Byp)
If I switch the 'TX_Byp' off, I can get the 'built-in' DAC test loop registers to out a pattern so that seems to imply that have a good DAC clock chain however, there is a note on pg 22 of the datasheet that states that in loopback mode, 'it is still required to give an active DAC_DCLKIN because the TX FIFO requires it for proper data transfer'. This is somewhat confusing to me and seems to imply that I still need to inject a signal on the 'DAC_DCLKIN' via the J21 SMA connector (after install R94 / R95 and removing R64 / R93) which I have tried, but to no avail.
Can anyone please provide some insight as to how to get the EVM module running in the 'RX-TX' loopback mode?
Thanks,
Chris Laatsch