Hi team,
My customer is considering to use the ADS8866.
Could you help with the questions below?
1. Is the 1/fsample of ADS8866 1000ns(min) or 10000ns(min)?
2. Tconv is specified as 500ns(min) to 8800ns(max). Does it mean that Customer can set the Tconv arbitrary within the range of 500ns to 8800ns?
3. What happens if Tconve exceeds 8800ns(max)?
4. When the Tsclk is 15ns(min), sclk * 16 = 240ns. Since the min of Tacq is 1200 ns, does the CONVST need to be held low for 1200ns even after finishing sclk output?
Regards,
Yamaguchi