DAC34H84evm with TSW1400 setup w/ output of data sampled at 781Khz - .csv pile 'playback'
I want to play back .csv data that was captured at a sample rate of 781khz with the DAC34H84evm on all 4 DAC channels:
Questions: From previous forum discussions it appears that the output transformer 'on board' will not pass lower frequencies (say <~75khz). Where is the information regarding the current transformer so that I can design/obtain a transformer more suited for the frequency range of ~2Khz to ~800khz?
Also, will the DAC actually work down to these low frequencies (disregarding the transformer issue)?
Do you have some guidelines for setting up for these low frequency ranges?
What about the 5pf output cap relating to the DAC output - Is there a way to make the DAC output characteristics more appropriate for use at <1Mhz???
Thank you,
DMV