Hi,
I am a bit confused as to what the full scale differential input swing of the ADC is. The datasheet clearly states that it is 2Vpp when ADC programmable gain is 0dB and 1Vpp when gain is 6dB which makes sense.
Now the supply rail is recommended to be at 1.8V (single). Is it normal for the ADC input swing to be that high given the supply rail at 1.8V?
Is the differential input swing related to the AVDD?
For example, if the AVDD is 1.8V then the digital outputs will send 4095 when the differential input swing is 1.8Vpp, if the AVDD is 1.9V then the digital outputs will send 4095 when the differential input swing is 1.9Vpp and so on as long as absolute maximum ratings are not violated.
Is that what it is?
Pls confirm
Best regards
Manos Tsachalidis