Hello team,
my customer is running the device in high resolution mode with 5V on AVdd and 3.3V DVdd and has the following questions.
1) What is the absolute max power dissipation the part can handle? The spec shows power dissipation in various modes and after 50krad exposure but what is the max dissipation the part can handle?
2) Is the AVdd current draw related AVdd? i.e. The max current listed is 11mA but is that at 5V or 3.3V? And is it more or less at higher voltages?
Thanks!
Errol