Other Parts Discussed in Thread: LMX2615-SP, TSW12D1620EVM-CVAL, LMX2594
Hello,
We wish to provide the sample clock to two ADC12D1620QML-SP devices using one LMX2615-SP device (using the RFoutA and RFoutB outputs)
1. Has anyone done this, at least for one channel, and can provide performance data (i.e. ENOB) from the ADC? Most concerned about internally generated spurs due to input clock
2. What is the required termination between the LMX2615 device and the ADC12D1620 clock inputs? Is a transformer required, DC network, AC coupling, etc?
3. Is a band pass filter recommended for the input clock to minimize harmonics of the input clock?
4. Is there a reference design or block diagrams that show the interconnections?
Regards,
John