hi dear supporting team,
customer is using ADS8320 with below sch(share the same circuit with AD7683). They found there is close to 1V glitch at Vin pin, which has same cycle with Cs signal. the input is disconnect with previous stage. and the sample rate is several 10KHz, Vref is 2.5V. I checked the sch, seems only decoupling cap mis-match with our recommend sch, will that be a issue? any other possible cause? tks a lot!
the CS and the glitch detect at Vin: blue is Vin, yellow is CS.
the CS&CLK timing: