Other Parts Discussed in Thread: DAC5571
Hi Sir
May DAC60501 can support I2C in and output 25KHz square waveform output?
Bogey
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Chen,
DAC60501 supports fast plus mode I2C which goes up to 1MHz SCL. The interface requires a 4-byte transfer for each update which, including ACK bits, would be a 36 bit transaction. 36 bits at 1MHz provides a maximum update rate of 27.77kHz - so the maximum square wave frequency in I2C mode would be ~13.9kHz.
Is 12-bits of resolution required for this application or might 10-bits or 8-bits also be acceptable?
Hi Kevin,
Thanks for your answer.
The 8-bits also be acceptable. Which DAC with I2C interface can support 25 KHz square waveform output?
Regards,
Roger
Roger,
We would need to take this part of the discussion offline as this is currently guarded by an NDA. Would it be okay to reach out to you at the email address that you used to register your myTI.com account with?
Hi Kevin
May we check again if there have other device can support without NDA request?
Bogey
Bogey,
Having scrubbed the portfolio a bit deeper DAC5571 may be able to work for you as it both offers the 3.4MHz high-speed I2C functionality and all updates after the first write can be executed using a 18 clock-cycle update routine. Between having more than 3x I2C clock speed and halving the number of clocks required for an update you can realize up to an 94.44kHz square wave.