This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC12DJ5200RF: Migrating from ADC12DJ3200 to the ADC12DJ5200RF

Part Number: ADC12DJ5200RF
Other Parts Discussed in Thread: ADC12DJ3200,

Hello,

    Our original design was done with the ADC12DJ3200 Analog to Digital converter. But due to change in specs, we decided to replace the ADC12DJ3200 with the faster ADC12DJ5200RF. The datasheet says that these two part are pin compatible and that the ADC12DJ5200RF has a higher power consumption. Power is not an issue on our design. However, when we built our board with the ADC12DJ5200RF, it fails with a JESD sync error right from the start. We are running the same test code on both ADCs. My question is: Are these two ADCs functionally and firmware compatible as well meaning if we have code for the ADC12DJ3200, will that work without modification with the ADC12DJ5200? Our first goal is to establish functional equivalency between the ADC12DJ3200 and the ADC12DJ5200RF before we move forward with the latters' more advanced functions. Your input on this issue will be much appreciated. Thank you.

-Dhruva