This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC081C021: ADC081C021 circuit check

Part Number: ADC081C021

Hi Sir 

The I2C will go through Isolators & Level Shifter, then into CPU.

For our circuit, application is 24V divided into VIN

Need to adjust the resistance part?

Is Address should be 1010100 ?

Is there need other note in the circuit?