Hi,
I am using the 12 bit ADC ADS7043 IC, in that I am measuring the current AVDD+DVDD but its taking around more than 10mA current.
Input supply voltage is 1.8V(AVDD & DVDD).
Input AINP=0.3V
Input AINM=0.9V
SCLK=1MHz
SDO trace capacitance is 5pF.
What is the cause of issue for damaging the chip.
This chip has low power device?
then what is current I_AVDD? , I_DVDD?