Hi,
I’m using DAC3171 in 7-bit mode,but finding that the lower 7 bits seems not showed because the noise floor is much higher. I think DAC3171 does not work in the 7-bit mode properly.
and I have found that the Bit 6 of config5 is always 1,the problem is that if Bit 6 of config5 is 1, the Bit 5 of config5 also should be 1 according to Table 12 in datasheet of DAC3171,but actually it's 0.
check the da_clk input to pin6 and pin7, the clock is OK.
I suppose that my power up sequence is not right。
should I provide the DACCLK and DA_CLK to the DAC3171 first,then config the DAC3171 register ?
The dac3171 register configuration is as follow:
0x00 0x6EC
0x01 0x401E
0x02 0x3F80
0x03 0x1C71
0x08 0x6000
0x09 0x8000
0x0A 0xF080
0x14 0x0000
0x01 0x401E
0x01 0x403E
0x01 0x401E
This problem has confused me for three days, pls give me some advice.
I'm looking forward for your reply,thanks a lot.