Part Number: ADS1110
Other Parts Discussed in Thread: ADS1115
hi, i have couple questions when using ADS1110 convertor.
1. seems like there are no Sample & Hold funtion for this devices, so what happen if the intput voltage change when converting?
the current setting is PGA=8 and DR=15 SPS 16 bit converting.
how long will this devices take to converting the analog voltage to digital number?(PGA=8 and DR=15SPS 16 bits)
2. about offset error
i need some detail information of how we deal with this offset error.
my input voltage range is about -0.5mV ~ 35mV, 0.4mV offset is somthing that i can not ignore.
So , is the error are fixed value for each individual components? like can i set a number in my CPU to corrector 0 point or i have to calibrate the ADC when power up?
3.What happen is Vin+ and/or Vin- goes higher than Vdd?
the analog sensor are working @ 5V but ADS1110 been set to working at 3.3V which will be easier to talk to CPU via IIC.
4.is there are CMRR and PSRR value can be guaranteed? since it's a differentail input signal and may have noise on 3.3V power source( like IIC clock and data line).
Thanks and best regards,