Part Number: DAC7554
Can DAC7554 be powered with VDD = 3.3V, but REFIN = 5V?
I think REFIN needs to be less than VDD for typical operation since the output buffer is powered by VDD.
However, if the DAC input was restricted such that the output voltage would never be programmed above VDD, is this acceptable?
Or maybe there are other internal paths to be concerned about such as ESD diodes between REFIN and VDD that would conduct under this condition?