Tool/software: Linux
TLA2024 AIN1 is connected to the NTC thermistor, we are using the TLA2024 12 bits value from Conversion Data Register .
I used below formula for converting the temperature in degree Celsius but i am not getting the exact temperature.
1/T = 1/T0 + 1/B * ln( ( adcMax / adcVal ) – 1 )
here T0 is the 25°C value in kelvin
B value is 3455 of the 10K ohms.
adcMax 4095 and adcVal is 12bit Conversion Register data.
can you please check, am i using correct formula?
if it is not correct please suggest to me, which formula I need to use here?