I recently bought a AD8363EVM, which I'm currently trying to interface via an SPI controller (FT2232H), I noticed unfortunately
the power connector J4 isn't labelled, so I tried to deduce the pins from the schematic and PCB traces. I can upload a photo of the connections I made if that helps diagnose my problem.
I tied A0- and A1- to GND. And A0+ and A1+ to 5V. And provided an external reference of 2.5V and disconnected jumper JP3 to achieve this.
I'm following https://www.ti.com/lit/ds/symlink/ads8363.pdf
#include <stdio.h>
#include <stdlib.h>
#include <mpsse.h>
int main(void)
{
int retval = EXIT_FAILURE;
struct mpsse_context *adc = NULL;
if((adc = MPSSE(SPI0, TEN_MHZ, LSB)) != NULL && adc->open){
printf("%s initialized at %dHz (SPI mode 0)\n", GetDescription(adc), GetClock(adc));
int z = 0;
for (z = 0; z<2; z++){
Start(adc);
char Txdata[4];
Txdata[0] = 1;
Txdata[1] = 0;
Txdata[2] = 0;
Txdata[3] = 0;
unsigned char * r = Transfer(adc, Txdata, 4);
if (r != NULL) {
int i = 0;
for (i=0;i<4;i++)
printf("%d\n",r[i]);
}
Stop(adc);
}
} else {
printf("Failed to initialize MPSSE: %s\n", ErrorString(adc));
}
Close(adc);
return retval;
}