I am having a load-cell connected with ADS1230. ADS1230 is interfaced with 8bit STM8s controller. while operating system on 5V, ADS1230 is giving 0xFFFFF value, i'm not getting the conversion as per loadcell voltage changes. While operating on 3V3 voltage, everything is working fine. In my schematic I want to operate whole system on 5V instead of 3V3. I'm not getting what is going wrong.
I need to get it resolved as soon as possible. Any comments or guidance highly appreciated.