This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS7263: Can ADS7263 be used for 8 singled ended analog signals?

Part Number: ADS7263

Here is a simple question regarding the ADS7263 converter. Please confirm if I can use this device to sample 8 single ended input signals referenced to AGND. In this case, if I connect CMA and CMB pins to AGND do I end up with full range of values for analog inputs from 0 volts to VREF or only half of the ADC range?