Can you help explain the differences between these devices?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can you help explain the differences between these devices?
Here are the key differences between these devices:
ADS1281 - This was the first ADC in ADS128x product family.
ADS1282 - Integrated a PGA & MUX in front of the delta-sigma modulator.
ADS1283 - Changed to a smaller package, reduced device's power consumption, added an internal offset to move idle tone, and added a /CS pin.
ADS1284 - Added an optional reduced power mode (from 18 mW to 12 mW). SNR in the low-power mode is reduced by 3 dB.