Tool/software: Code Composer Studio
Hello everyone... I was trying to use the ADS1191 for a project but I got confused with the power supply. the datasheet says that I hace to connect two power sources to the ADS1191 but I wonder if I could conect a source with the same value to the device... There is an example of connecting the Device to Unipolar (+3 V/+1.8 V) Supplies in page 53 but I was thinking Could I connect one power supply to both AVDD and DVDD?. I'd like that someone could help me with this doubt. I am goint to left a image with the datasheet conection, and I am going to draw the conection that I think could be correct.