Part Number: AMC1304M05
Other Parts Discussed in Thread: AMC1210
Hi team,
I am helping customer to test AMC1304 together with C2000. Thus I am trying get some detailed knowledge on this devices.
When I am looking into the resolution of AMC1304, it makes me a little bit confused.
The question is about the following figure:
Assuming we are using a OSR=10. For Sinc1 filter, it is easy to understand the max number of "1" sampled will be 10, thus the resolution will be ~3bit which matches the figure.
However, for OSR=10 Sinc2 filter, according to my understanding, the max number we are getting is actually 100 (10*10) which brings a 6-7 bit resolution. And this does not match the figure.
Could please help to correct my understanding on this topic?
Regards,
Brian