This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS5402EVM: Is the schematic same with the already-obsolete ADS540"1"EVM?

Part Number: ADS5402EVM
Other Parts Discussed in Thread: ADS5401,

Hello,

Our customer is looking for the schematics of ADS5401EVM because they will use it as reference for their design using ADS5401 (still active). However, upon checking, the EVM is already obsolete and the documentations are no longer available for access.

(1) Would it be possible to request from you the schematics of ADS5401EVM?

(2) If it's not possible, is the schematic of ADS5402EVM entirely the same as ADS5401EVM?
We've seen that ADS5402EVM can be used to evaluate ADS5401, and I was wondering if they can use its schematics instead. 


Thank you!