Part Number: ADS125H02
Other Parts Discussed in Thread: ADS1262, DAC8775
Hi Sir
We would like to use ADS125H02 to measure +/-10V and +/-20mA
May I know have any reference design or circuit could be refereed ? especially -20mA
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Kai,
We have short tech doc on using the ADS125H02 for +/- 10V measurements here: http://www.ti.com/lit/an/sbaa387/sbaa387.pdf
For current measurements, we don't have any reference designs specific to the ADS125H02, but we do have some reference designs for a similar device (the ADS1262) which would likely be just as relevant except that for the fact that the input range on the ADS125H02 is much wider. See http://www.ti.com/tool/TIPD164 and http://www.ti.com/tool/TIDA-00550.
I hope that helps!
Hi Kai,
It looks like the current source is applied between pins 2 and 3 on J1, and the current is measured as the voltage drop across the R25 burden resistor, is that correct?
I don't see any issue from the circuit as you've drawn it. Some times there may be a TVS diode across the burden resistor to protect it in case of mis-wiring. Just take care to ensure that the burden resistor's power dissipation is never exceeded in case of an electrical overstress (EOS) event.
Also, if you haven't already, I'd recommend taking a look at the ADS125H02 Design Calculator (Rev. A) to double check that the input common-mode voltage is within range of the ADS125H02. With the wide input-range of the ADS125H02, it shouldn't be an issue.
Hi Kai,
FYI: Collin recently posted an additional reference circuit for the ADS125H02 over on this E2E thread, which you may find applicable to your design: