I want to use ads4129 adc with Raspberry pi4. I want to learn if they are compatible and need any extra file for interface contact.
Thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I want to use ads4129 adc with Raspberry pi4. I want to learn if they are compatible and need any extra file for interface contact.
Thank you
Serkan,
We have not interfaced these two boards but with some work, I think you could if the Raspberry can receive 1.8V CMOS logic level inputs. The ADS4129EVM would require a CMOS buffer and two rpacks to be installed and two rpacks removed to setup the EVM for 1.8V CMOS outputs (it is LVDS by default) . You then would have to build a custom harness to connect the ADS4129 CMOS outputs to the GPIO connector of the Raspberry board.
Regards,
Jim