Hi,
I did experiment to check if the EVM converts data properly by measuring DAC output and ADC input.
When i checked the DAC output after modified program DAC voltage, i could get the voltage what i put.
However, when i checked the program ADC voltage after supplying voltage to ADC input, I could not get the voltage i supplied.
For example, when i supplied 4V, I could only get 3.1V. When i supplied 1V, I could get 1.4V. (Default voltages are about 2V)
Only in ADC_input 2,3, i could get the exact voltage i put.
I think this is because there are buffers in front of ADC_input 2,3.
But, I wonder why the buffer makes this difference.
Also, I wonder how i can get the exact voltage i supplied except ADC_input 2,3.
Also, I wonder why there is default voltage around 2V when there is no voltage supplied?
thanks,