Hello,
Sorry if this question is quite rudimentary, but if you are using the ADS7952 and wish to use the High and Low alarm related GPIO's, what external components do you attach to these pins? The pin can go high and low, so does that mean you just put a resistor to gnd on both pins (ensuring the 10ma spec isn't surpassed), and that the pin voltage is held (for example) at 2.5VDC, so that a high is 5VDC and a low is around GND?
Cheers