Other Parts Discussed in Thread: ADC12DJ3200, , ADC12DJ5200RF
Hello,
We are intending to use the ADC12DJ3200EVM to under sample signals above Nyquist, and are therefore interested in the full frequency response of the ADC. The specification of the ADC12DJ3200 claims usable input frequency range of >10 GHz. However, in Figure 14 of the attached data sheet for the ADC12DJ3200EVM eval board, there are strong ripples observed above 3GHz. We have also measured these ourselves in the lab. Such ripples are not observed in the data sheet for the ADC12DJ3200 alone.
Our concern is that these ripples are due to impedance mismatches on the EVM board at frequencies above 3GHz. If so, this will have negative impacts on our system performance.
We would like to get answers to the following questions:
1) What is the source of these ripples?
2) Is there a way we can reduce these ripples in the frequency response of our ADC12DJ3200EVM though a hardware fix or other modification?
3) Does TI offer other solutions, or can they recommend other eval boards, that have a smoother frequency response across the full frequency range of the ADC12DJ3200 (DC-10GHz)?
Thank you,
Brandon Buckley