Other Parts Discussed in Thread: TSW14J56EVM, TSW14J57EVM
We need to evaluate the ADC performance of as TI GSPS ADC in combination with the TSW14J56EVM/TSW14J57EVM and Data Converter Pro software.
Our tests require to analyze a huge variety of input signals, thus we need some automation of the Data Converter Pro software. It would be sufficient, if the software can be triggered to start a new aquisition and exports the acquired data to a file. All settings of the ADC remain unchanged and can be made manually via the GUI. We would just need a way to control this in an automated way, e.g., sending a byte to a TCP/UDP port or using an API. It could be even a hardware trigger sent to TSW14J56EVM board which would be most preferable, meaning a new recording file is generated whenever a trigger signal occurs (of course, I would ensure that enough time is in between two events as reading the data over USB3.0 and writing it to disk will take quite some time)
Is there any way to accomplish this with the software?
BTW: having this functionality in output direction (proving a DAC data file) and updating the DAC data in an automated way might be also a useful feature in near future for us.