This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC53401: typ/max current draw at 3.3V

Part Number: DAC53401


Hi,

What is the typ/max current draw of this device with a 3.3V supply?

Thanks,

Jose

  • Hello,

    Please refer to page 6 of the datasheet, "IDD - Current flowing into VDD". There are two conditions, normal mode and power-down mode. In normal mode the typical and maximum specifications are 0.5mA and 0.8mA, respectively. The conditions column indicates that the digital I/Os were inactive and the DAC was set to full-scale.