This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8904B: SCK capacitance

Part Number: ADS8904B


Hello,

Can we please request for the expected input capacitance of the SCK pin?

Also, by adding a series resistance to the SCK input, can it possibly reduce/prevent the SCK clock noise from coupling to the ADC inputs?

Thank you!

  • Hello Elisha,

    The digital input capacitance is included in the IBIS model.  You can download it here:

    http://www.ti.com/lit/zip/sbam305

    Open this file in a text editor, and you can find the capacitance for the specific IO pins.

    It looks like input capacitance C-comp is 0.38pF, and the package capacitance is 0.2pF.  You will probably have an additional 1pF of capacitance due to the board as well.

    Yes, adding a series resistance can reduce SCLK noise.  We usually include series resistors (50ohm) on all of the digital control lines on the TI EVM's just in case. Many times they are not needed, but depending on the board layout and the MCU/FPGA drive strength, there are cases where these resistors are very helpful.

    Regards,
    Keith Nicholas
    Precision ADC Applications 

  • Thanks a lot, Keith! One more question though -- does that mean that the total input capacitance of the SCK pin is the sum of all three?

  • Hello Elisha,

    The input impedance is more complex, with resistance and inductance as well as capacitance.  However, for a simplified analysis, I normally just add all of the individual capacitance values.  Using this total capacitance value, and any external series resistance, will give an estimation on rise/fall times.

    Thanks,

    Keith