Other Parts Discussed in Thread: TMDSDOCK28379D, ADS8686S, ADS8588SEVM-PDK, LAUNCHXL-F28379D, ADS8588S
hi
i would like to know if i can Interfacing 7 channel from ADS8686SEVM-PDK Evaluation Module with F28379D Delfino Experimenter Kit (TMDSDOCK28379D)
and if it possible to Connect LCD to the same board (F28379D Delfino Experimenter Kit TMDSDOCK28379D). If possible, which LCD is okay? .
My application is to build numerical relay that can take at least 7 simultaneously analog input the board must connected to LCD for human interface, the board also must able to connect to Ethernet to take information from the cloud , the board also must have output signal to circuit breaker in case of a fault ....so with these a lot requirement i need multi-board interfacing.