Hi E2E,
Good day.
Our customer would like to know what transformer should be used for a driving circuit above 270MHz? From the datasheet (http://www.ti.com/lit/ds/symlink/ads4249.pdf), it was stated that ADTL2-18 transformers can be used for the Figure 76 configuration, however, the figure shows two 1:1 transformer, but the ADTL2-18 is a 1: 2 transformer. Can you please advise on this?
Thank you in advance for your help.
Regards,
Carlo