Other Parts Discussed in Thread: STRIKE, ADS1278
On a number of occasions, I've run into the part locking up. The symptom initially is that the sampled data comes back with all zeros. On closer inspection, the part is drawing a very large amount of current (about 100mA), and heating up significantly. Due to some RC filters in the AVDD path, this high current draw drops the AVDD to the part down to about 2 volts (maybe 2.5, I don't recall exactly). I measured over 1V drop on the 10 Ohm resistor, so that's where the 100 mA number is derived. Once this condition happens, power cycle returns everything to normal.
There is a spec in the data sheet about "momentary" 100 mA current draw. What is that? I will guess it's during the conversion process. This seems to be when the part locks up as well.
Thinking that the device is in a latchup state, I removed the 10 Ohm resistors thinking that the power rail will no longer droop. Yet, during some conversions, the device returned all zero again. The power rail holds tight at 5 volts now, but I do not know how much current is drawn.
Is this a known problem, or perhaps we have this chip connected poorly.
thank you.