This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC8551: Datasheet Figure 32 source and sink capability - Value missmatch?

Part Number: DAC8551
Other Parts Discussed in Thread: DAC80501, ,

Dear TI support team,

Comparing Figure 32 the curve zero voltage sink capability of the DAC8551 datasheet with DACs having a compareable output stage (see DAC80501 for example) , the valures presented in DAC8551 are factor 1000 or more better. Additionally if you have a close look on the curve for max. output voltage (2.7V - 10mV ) and you look on the y-axis, you have 2,7mV (instead of something in the range of 2.7V). Is there a typo? From my understanding "V" instead of "mV" as y-axis would give a more realistic picture.

Can you please support here?

Best regards,

PS: Same sitaution on DAC8551-Q1 for example