This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS7951-Q1: ADS7951-Q1 ADC unused pins recommendation

Part Number: ADS7951-Q1
Other Parts Discussed in Thread: ISO7721

Hello All,

1.what is the Ti recommendation for ADS7951-Q1 ADC for the below pins?

1.Unused GPIO

2.NC pins

3.Unused ADC Channel

2. what is the Ti recommendation for  unused channel in the ISO7721?

Regards,

Bhupathi

  • Hello,

    I would suggest the following:

    1. These can be grounded

    2. ADC input should be grounded

    The way the forums are looked are by part type. Once your ADC questions are answered, I can push this to the team that supports isolation part.

    Regards

    Cynthia