Part Number: ADS1115
I am trying to measure a 70 VDC (very limited power source. Aprox 3 mA) with very high precision. I used a resistor voltage divider (8.2 MOhms and 536KOhms) a buffer with an op/amp (gain 1) and an RC filer as front end for the ADS1115, but I get a very low frequency (20 s) noise on top of the DC sample signal measured that is not on the 70 VDC input signal. I tried changing the cut off frequency of the RC filter before the ADS1115 but due to the very lo frequency, the overall response of the circuits becomes several minutes. This prevents using the measured signal to control the generation of the 70 VDC signal
Any ideas?