This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC1306M25: Read data DOUT Pin.

Part Number: AMC1306M25

Hello~

I have three questions.

Question 1.
-> When a single clock is generated by the MCU, The AMC1306 is output in bitstream form via the DOUT pin.

    Is it correct to receive 1 bit from the MCU as a digital input?

    If not the above method, what form should be read?

Question 2. (When supplying 0 -> 3.3V to AVDD)

   - How many clocks should be generated after tSTART (500us)? (128 CLOCK ?)

Question 3. (AVDD always supplied)

  - I would like to know how to distinguish one cycle of effective bitstream .