Part Number: DAC8562T
Other Parts Discussed in Thread: DAC8562
Hello,
I'm encountering some issues with the DA8562T.
When I start sending data to the DAC, the Vrefout become crazy. It rise above 2.5V (to 3v3 which is our Vsupply), or fall to 0V. Unnecessary to say that the output isn't working properly :
Yellow is nSYNC / Blue is clock (~4.5MHz so not enough samples to see it here), and purple is Din. While I send zeroes, everything is ok, and when I start with data, Vrefout problems start (green).
Next to that, if I plug the evaluation board in parallel, with the same supply and same communication BUS in the same time, it's working and my output is ok on eval board.
The only differences are on nLDAC and nCLR which are not the same, but I tried different solutions (0v, pull-up, cpu controlled); nothing change.
And the component footprint (VSSOP on my board).
I did a lot of different tests to find the problem (replacing component, checking supplies, using external reference, send power-on reset command)
I disconnected both output, tried multiple capacitor (on vref and vdd)
Schematic :
Data bus looks good enough :
An other vrefout drop :
Thank you, if somebody can help me to find a solution, or a way to find the problem...