This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC38RF82EVM: high phasenoise of DAC38RF82/90 with internal PLL

Part Number: DAC38RF82EVM
Other Parts Discussed in Thread: LMX2594, DAC38RF80

Dear forum members,

 

we do have the problem of high phase noise / jitter when using the DAC38RF8x internal PLL.

We would like to get information where root cause of the high the phase-noise could be.

 

In the attached document different measurement setups and the

phase noise plots at 1845MHz output frequency are shown.

The DAC sampling frequency is 9GHz on each setup.

Setup 1 shows our design with DAC and external PLL running at 9 GHz (LMX2594).

Setup 2 shows our design with DAC internal PLL and external 250 MHz reference.

   This we would like to use.

Setup 3 shows a setup with DAC38RF8x EVM and external 250 MHz reference based on our design.

Setup 4 shows a setup with DAC38RF8x EVM and external high quality 250 MHz reference SMBV100b.

 

It can be seen that the DAC with internal reference can run with much better phase noise output

than on our prefered setup 2.

 

We would like to get information what the root cause for the high phase noise could be.

Where could we search for the reason?

What could be the root cause of the higher PN in the range of 10k to 300k?

There is a peak of about 10db at about 60kHz.

The origin of this we also did not detect up to now.

 

We already changed/increased charge pump current in the DAC PLL but this did not

improve phasenoise remarkably.

 

Thank you for your help and best regards

Christoph

Test-Setups.pdf

  • Hello Christoph,

    I have looked at the measurement briefly and have some preliminary recommendations/comments:

    1. Typically, the PLL performance will improve with increased PFD frequency. The DAC38RF8x family supports up to 500MHz of PFD. Could you please increase your reference clock to the DAC PLL to 500MHz (with decreased M divider) to see if the phase noise could improve?

    2. My understanding of the problem is the peaking at 60kHz or so of phase noise performance. Your far end noise actually looks better (on the blue curve) when compared to the EVM (on the yellow curve). A couple suggestions:

    a. Check if there are any switching frequencies of DC/DC power supply switching around 60kHz or so. If so, see if you can improve shielding from the switching power inductor to the DAC. The most frequent coupling of the double side band noise is due to the magnetic coupling of the power inductor to the DAC PLL inductor ring within the device package

    b. pay attention to any ferrite bead or power supply filters that can potentially resonate at 60kHz.  . If possible, remove these filters or inject an external, high quality analog power supply to the power supply group and retest. Please note that you have to inject high quality analog power supplies. Some bench supplies are still digital control based with digital feedback, and may create some additional noise

    c. check if the PLL is locked correctly. Follow these steps as guideline to ensure PLL lock

    Questions:

    1. The custom board that you have, how is the routing done, especially for the PLL power rails and the clock input path? Are there any potential coupling mechanism?

    2. which part are you actually going to be using? 82, 83, or the 90? Different parts may have different PLL/VCO range. This may be a problem in terms making sure the PLL frequency is locked and centered

    3. I saw on your custom design measurement (blue curve) has warning mentioning set att = 0dB on the E5052. Could you please double check and confirm as this may limit your noise performance measurement?

  • Hello,

    we will close this forum post for now. I believe you are still working on a few measurements to check on the PLL performance improvement. Please feel free to reply back to the post to re-open the discussion.

    -Kang

  • 1. Typically, the PLL performance will improve with increased PFD frequency.

    The DAC38RF8x family supports up to 500MHz of PFD. Could you please increase your

    reference clock to the DAC PLL to 500MHz (with decreased M divider) to see if the phase noise could improve?

    The 250 MHz PFD frequency is the highest frequency we are able to use in current custom design.

    We’ve tested the same configuration at DAC38RF80 EVM and see DAC38 is performing well there.

     

    2. My understanding of the problem is the peaking at 60kHz or so of phase noise performance.

    Your far end noise actually looks better (on the blue curve) when compared to the EVM (on the yellow curve).

     

    A couple suggestions:

     

    a. Check if there are any switching frequencies of DC/DC power supply switching around 60kHz or so.

    If so, see if you can improve shielding from the switching power inductor to the DAC.

    The most frequent coupling of the double side band noise is due to the magnetic coupling

    of the power inductor to the DAC PLL inductor ring within the device package

    There are not used circuits (DC/DC or similar) which use switching frequencies around 60kHz.

     

    b. pay attention to any ferrite bead or power supply filters that can potentially resonate at 60kHz.

    If possible, remove these filters or inject an external, high quality analog power supply to the

    power supply group and retest. Please note that you have to inject high quality analog power supplies.

    Some bench supplies are still digital control based with digital feedback, and may create some additional noise

    We exchanged the currently used ferrite bead with the EMI filter NFM31PC276B0J3 which is used on Eval. Board.

    This helps to improve the 60kHz peaking and lowers the phase noise for a bit but it’s still

    about 8dB higher at marker 6 (green curve in the attached document).

     

    c. check if the PLL is locked correctly. Follow these steps as guideline to ensure PLL lock
    The PLL is locked correctly.

    It was "locked manually". We incremented/decremented

    the VCO tune value and set it in the mid of stable area.

    We also connected the SPI bus of the EVM to the DAC on our design and controlled

    and configured the DAC with the TI GUI in the similar way the configuration has been done

    on the EVM. So the configuration and also PLL locking seems not to be an issue.

     

    Questions:

     

    1. The custom board that you have, how is the routing done, especially for the

    PLL power rails and the clock input path? Are there any potential coupling mechanism?
    Would you mind taking a look on the layout? We do not want to post it to the forum.

    If you have time to take a look on the layout we would like to send it to you

    directly.

     

    2. which part are you actually going to be using? 82, 83, or the 90?

    Different parts may have different PLL/VCO range.

    This may be a problem in terms making sure the PLL frequency is locked and centered

    Actually we are using the 83 with external PLL.

    We plan to change to 90 with internal PLL.

    We performed the internal PLL tests with both 83 and 90.

     

    3. I saw on your custom design measurement (blue curve) has warning mentioning set

    att = 0dB on the E5052. Could you please double check and confirm as

    this may limit your noise performance measurement?
    We checked the warning it had no influence to the measurement results.

     

     

     

     

    Thank you and best regards

    Christoph

     

     

    Test-Setups_2.pdf

  • As layout file is being shared, we will discuss this offline with customer and closing this thread.