Part Number: ADS8350
Hi guys, can anybody confirm for me the numbers used for the SNR calculation?
A customer I have is asking about how SNR was actually obtained.
I am attaching an image below for reference but this is what I have so far...
- This is a pseudo-differential ADC, so AINM is held at VREF (2.5V), while an AC signal with DC offset at VREF(2.5V) is applied to AINP (actually only -0.5dBFS)
- In this case, the signal has a Vp-p of around 4.72V (-0.5dBFS for FSR of 5V), correct?
- Thus, since the calculation for SNR is 20LOG(Vsig_rms / Vnoise_rms), we calculate Vsig_rms as (4.72 / 2√2)
- After we find this, by using TYP SNR at 84dB (from DS), we can calculate the Vnoise_rms during the test.
Is this how SNR was calculated? (Vsig_rms as 4.72 / √2)