This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC12DJ3200: Clocking scheme with LMK04832

Part Number: ADC12DJ3200
Other Parts Discussed in Thread: LMK04832, LMX2582

Hello, I'd like to run an idea by the experts here and see if it makes sense.

I'd like to do a design with a single ADC12DJ3200 running in Subclass 0. I'd like to use the LMK04832 in a single-loop configuration. I'd use VCO1 so that I can clock the ADC directly at 3200 MHz and then feed the MGT reference clock at 160 MHz. Does this sound reasonable?