Other Parts Discussed in Thread: REF02, ADS1110, ADS1118, ADS1115
Hello there,
my question is directed at AD converters ADS1100 that draw their reference voltage from Vdd. In other words, supply voltage is the reference voltage and as that should be precise and stable.
I'm working on an existing design where one MAX6195AESA+ voltage reference (Vin= 12 V, Vout = 5V, load current max. 0.5 mA, temp coeff vout = 5 ppm/°C, ripple rejection 72 db, load regulation 0.7mV/mA) powers two ADS1100 in single ended configuration (15 bit). Now the datasheet of MAX6195AESA+ states that it is stable with capacitive loads up to 2.2nF. However, the datasheet of the ADS1100 recommends to place 100 nF bypass capacitors between Vcc and GND: when converting, the device draws current in short spikes. The bypass capacitor supplies the momentary bursts of extra current needed from the supply.
So in the existing design the MAX6195 sees 200 nF capacity at the output which obviously does not meet its specification.
I'd like to improve this design. FYI, the application does not rely on measuring absolute values precisely but relative values, i.e., measured values should be stable without drifting over time or temperature.
Could you please recommend a voltage reference that is sufficiently precise and stable to drive two ADS1100. For example, is a REF02 stable enough for maximum AD precision (within one LSB)?
Alternatively, which AD converter would you recommend to replace the ADS1100 which includes a voltage reference (and is at least as precise as the ADS1100).
Thanks.
Best regards,
Dan