This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC80501: No DAC Output but other spi commands work

Part Number: DAC80501


I've been able to write to the Config register to disable/enable the voltage reference. So I know SPI is working.

On two separate setups, I have not been able to get the output to drive anything. I'm sending 0x08 0x8000 to set the device to midrail. Nothing happens, just 0V output.

I've tried on my application board and the TI EVM board.

Do I need to send another command to enable the output? I've tried using the Lsync feature, but that did not help either.

Thank you,

Tim