Part Number: ADS131A04
Hi team,
My customer considers to use 3pcs of ADS131A04 with multiple device configuration(all devices are operated as synchronous slave mode).
Then he provided following questions.
- Is the Initialization Set Up required for each device when connecting three ADC multiple devices?
(Do I need to do the same register settings three times in a row?) -
Fixed versus Dynamic-Frame Modes With ADCs Enabled Figure 54. b) Dynamic Frame Size (CRC Disabled)
Does the Status setting of DOUT come back every data? - Is it possible to use CLKIN=16.384MHz, SCLK=12.228MHz when connecting 3 ADCs with multiple device configuration?
I'm looking forward to hearing back from you.
Beset regards,
Shota Mago