Other Parts Discussed in Thread: ADS1130
Dear Sir,
I have used ADS 1130 for my Electronics WeighScale Application.
Although everything is working fine and readings are also stable, I am facing one typical problem which is described as under.
The ADC Count and hence the Weight gets disturbed and fluctuates a lot when evenever any of the Electrical Appliance connected to grid powered is Switched On and OFF.
Say in my lab or in my room I have powered the Weigh Scale from a 230V Wall Outlet and if any of the electricl appliance like a Flourescent Tubelight or Laser Printer or a computer or a Ceiling Fan or any such load connected in the Room is Powered On or Off the ADC Count and hence the Weight displayed fluctuates a lot. Possibly this is EMI interference or Electrical Noise affecting the system.
Pls advise and guide me in eliminating this noise to put the systems through and resolve the issue.
Rgds
Sulax
India
09427610356