Part Number: TSW1400EVM
Tool/software: WEBENCH® Design Tools
Hello I'm using TSW1400EVM and DAC34SH84EVM and I have the following problems using DATAConverter PRO and DAC34SH84 SW:
1) I have to run the APP as administrator otherwise it gives an error reading configuration files;
2) I can't generate more than one tone in dataconverter pro, the button to activate multitone generation is grayed why? This would be very important to me.
3) the EVB are correctly working with external clock while it deliver a very noisy and corrupted output when I try to use the DAC34SH84 EVB internal oscillator. I tried to use the examples contained in installation directory but the output is corrupted. Is there any simple procedure and configuration file I can load to check if all is working?
Thanks in advance for any of your answers
Luca