This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC7728: Interface with TMS320F28379D

Part Number: DAC7728
Other Parts Discussed in Thread: TMS320F28379D,

Dear Sir, 

I wanted to use DAC7728 with the controller. I need to know that the timing requirement of the DAC is compatible with TMS320F28379D or not ? 

Do I need more components to meet the timing for write operation into DAC ?

I made the circuit and i joint the address line to DAC and data line as given and regarding CS and Write I tide the lines EM1CS3 memory.

And I followed the datasheet instruction for pins configuration(as given in DAC datasheet). 

If the timing will not match then suggest the other parallel DAC which is compatible with TMS320F28379D. I need to decide this as fast as possible.

If there are some FAE that can help me please provide the no.

waiting for reply

Ashutosh Bhatt

7042391982