Hello,
I am planning to configure ADS42LB49EVM with an FPGA, the FPGA IO bank is using 2.5 volts.
Will the serial interface work with 2.5v? I have noticed the ADC can wok with 1.8 and 3.3 cmos levels but I didn't find anyway to switch between the two?
Also, does the eval board has a method to switch between controlling the spi lines via usb or FMC?
Regards,
Mahmoud